Ordering Information

A table is provided that gives the fully qualified orderable part number and topside symbolization for every package option of the device.

TI has converted to an advanced order-entry system that provides significant improvements to all facets of TI business, from production, to order entry, to logistics. One requirement is a limitation of TI part numbers to no more than 18 characters. Based on customer inputs, TI determined that the least-disruptive implementations would be as outlined below:

1. Package alias

TI uses an alias to denote specific packages for device numbers that exceed 18 characters. The Table  below shows a mapping of package codes to an alias representation.

2. Speed Indicator

For most devices of the same processor, the main difference between devices is the speed designator and the temperature capability.  The last set of numbers for the device will contain this information.  As in the table above, these parameters provide the maximum operating conditions for the device.