What should I do if I receive C6000 CCS-Compile Tools
V1.20 as an upgrade from EVM v1.0?
An error occurred in the Registration of the C6000 CCS EVM users. They have received the CCS-Compile
Tools upgrade for CCS 1.20 instead of the CCS-EVM Tools upgrade. The C6000 CCS-Compile Tools comes with
only Simulators, there are no emulation drivers in the upgrade CD.
After installing the CCS-Compile Tools upgrade, you will have only the Simulators as the option
in the CC Setup configuration.
Go to the following URL to download the self-extracting executable. The file will run and
Install shield contains a readme file which includes instructions and a description of which
files are being updated/fixed.
Download C6000 EVM patch.