BIOS and config file settings for XDS510PP emulator by Spectrum Digital.
The following are a list of BIOS settings and the related settings for the XDS510pp.ini file (for Code Composer 3.0x) and the sdopts.cfg file (for Code Composer Studio or Code Composer 4.xx). When setting up this hardware, please ensure these settings match or the user will run into setup and communication problems. BIOS SETTING | XDS510pp.ini file (for Code Composer 3.0x) | or sdopts.cfg file (for Code Composer Studio or Cc 4.xx)
-----------------|---------------------------------------------------------------
epp | epp or spp8
-----------------|---------------------------
spp or | bidirectional or | spp8 OS/2 |