Cannot initialize the TI emulator using emurst on a Solaris machine.

If there are problems initializing the XDS510WS emulator using the 'emurst' command, one thing to check into is whether the installation has been performed while being logged in as root. There could be a problem if another user is actually logged into the Sparc and then you use the "su" command to login as root. Although the documentation says that the installation should be performed as root, it does not specify that the user should be logged into the Sparc machine itself as root, and not use the "su" command from another user's login.