There is Flash memory on the 6211 DSK, can I reprogram it?
Yes, you can reprogram the memory on the C6211 DSK. While a separate turnkey utility is not provided, there is an example program called 'post' that contains all of the source code to reprogram the flash with the Power On Self Test. This source code, along with information under 6211 DSK help [lookup 'Flash Programming Utility'] can be used to develop a '.out' file that will program user code into the flash.