What Type of Filter Do I Need?

Problem:
What type of filter do I need?

Solution:
There are some questions that have to be answered while answering this question:

  1. What frequencies are wanted, and what frequencies are NOT wanted?

  2. How much rejection is needed on the frequencies that are not wanted?

  3. Which is important:

    • Amplitude
    • Phase
    • Delay

    or some combination of these?

  4. Is cost more important, or is the ability to make changes?

  5. What power supplies are available?

  6. How do I select R's and C's for a Filter Circuit?
The designer must diligently find the answers to these questions, or it will be impossible to design a good filter. If the designer has a good idea of what type of filter is needed, they can now select the intermediate level Filter Design Wizard or the advanced level Filter Expert.