Single-Supply Twin T High Q Bandpass Filter

Problem:
How does a designer make a Twin T High Q Bandpass filter that operates from a Single-Supply?

Solution:
Use the circuit below:



This circuit is most suitable for use as a high sensitivity single tone detector. Absolute levels of amplitude will be hard to obtain. High Q circuits like this can also be unstable, and it may be best to de-tune it slightly.

There are some general techniques to use with the Twin T topology that will greatly improve its performance: The designer, if not familiar with the topics, may want to review Coupling Capacitors (Cin in the schematic) and Virtual Grounding (Vcc/2 in the schematic).