Turn-On Voltage (shutdown) Parameter (VIH-SHDN or V(ON))

Problem:
What is meant by the turn-on voltage (shutdown) parameter (VIH-SHDN or V(ON))?

Solution:
The turn-on voltage (shutdown) parameter, VIH-SHDN or V(ON), is defined as the voltage required on the shutdown pin to turn the device on. It is expressed in units of V.

Also refer to the following related links:
Op Amp Parameter Table
Op Amp Parameter Information

These pages were extracted from Op Amps For Everyone, Chapter 11, by Bruce Carter, Ron Mancini–Editor in Chief.
Copyright © 2000, Texas Instruments Incorporated