Turn-off voltage (shutdown) Parameters (VIL-SHDN or V(OFF))
Problem:
What is meant by the turn-off voltage (shutdown) parameter (VIL-SHDN or V(OFF))?
Solution:
The turn-off voltage (shutdown) parameter, VIL-SHDN or V(OFF), is defined as the voltage required on the shutdown pin to turn the device off. It is expressed in units of V.
Also refer to the following related links:
Op Amp Parameter Table
Op Amp Parameter Information
These pages were extracted from Op Amps For Everyone, Chapter 11, by Bruce Carter, Ron Mancini–Editor in Chief.
Copyright © 2000, Texas Instruments Incorporated