Step Voltage Peak-To-Peak Condition (V(STEP)PP)
Problem:
What is meant by the step voltage peak-to-peak condition (V(STEP)PP)?
Solution:
The step voltage peak-to-peak condition, V(STEP)PP, is defined as the peak-to-peak voltage step that is used as a test condition for parameters such as ts. V(STEP)PP is expressed in units of V.
Also refer to the following related links:
Op Amp Parameter Table
Op Amp Parameter Information
These pages were extracted from Op Amps For Everyone, Chapter 11, by Bruce Carter, Ron Mancini–Editor in Chief.
Copyright © 2000, Texas Instruments Incorporated