Rise Time Parameter (tr)

Problem:
What is meant by the rise time parameter (tr)?

Solution:
The rise time parameter, tr, is defined as the time required for an output voltage step to change from 10% to 90% of its final value. It is expressed in units of s.

Also refer to the following related links:
Op Amp Parameter Table
Op Amp Parameter Information

These pages were extracted from Op Amps For Everyone, Chapter 11, by Bruce Carter, Ron Mancini–Editor in Chief.
Copyright © 2000, Texas Instruments Incorporated