Large-Signal Voltage amplification Gain Condition (AV)

Problem:
What is meant by the large-signal voltage amplification or gain condition (AV)?

Solution:
The large-signal voltage amplification or gain condition, AV is defined as the ratio of change in output voltage to the change in voltage across the input terminals that is set up for a test of parameters such as ZO or THD+N. It is expressed either unitless or in dB.

Also refer to the following related links:
Op Amp Parameter Table
Op Amp Parameter Information

These pages were extracted from Op Amps For Everyone, Chapter 11, by Bruce Carter, Ron Mancini–Editor in Chief.
Copyright © 2000, Texas Instruments Incorporated