Maximum Junction Temperature Parameter (TJ)
Problem:
What is meant by the maximum junction temperature parameter (TJ)?
Solution:
The maximum junction temperature parameter, TJ, is defined as the temperature over which the die may be operated. Some of the other parameters may change with temperature, leading to degraded operation at temperature extremes. TJ is expressed in units of °C.
TJ is listed in the absolute maximum ratings table because stress beyond those listed may cause permanent damage to the device. Functional operation to this limit is not implied and may affect reliability.
Also refer to the following related links:
Op Amp Parameter Table
Op Amp Parameter Information
These pages were extracted from Op Amps For Everyone, Chapter 11, by Bruce Carter, Ron Mancini–Editor in Chief.
Copyright © 2000, Texas Instruments Incorporated