Input Capacitance Parameter (Ci)

Problem:
What is the meaning of the input capacitance parameter (Ci)?

Solution:
The input capacitance parameter, Ci, is defined as the capacitance between the input terminals of an op amp with either input grounded. It is expressed in units of F.

Ci is one of a group of parasitic elements affecting input impedance. The following figure shows a model of the resistance and capacitance between each input terminal and ground and between the two terminals. There is also parasitic inductance, but the effects are negligible at low frequency. Input impedance is a design issue when the source impedance is high. The input loads the source.

Input capacitance, Ci, is measured between the input terminals with either input grounded. ci is usually a few pF. In the figure above, if Vp is grounded, then Ci = Cd || Cn.

Sometimes common-mode input capacitance, Cic is specified. In the figure above, if Vp is shorted to Vn, then Cic = Cp || Cn. Cic is the input capacitance a common mode source would see referenced to ground.

Also refer to the following related links:
Op Amp Parameter Table
Op Amp Parameter Information

These pages were extracted from Op Amps For Everyone, Chapter 11, by Bruce Carter, Ron Mancini–Editor in Chief.
Copyright © 2000, Texas Instruments Incorporated