Input Current Range Parameter (II)

Problem:
What is the meaning of the input current range parameter (II)?

Solution:
The input current range parameter, II, is defined as the amount of current that can be sourced or sinked by the op amp input. It is usually specified as an absolute maximum rating expressed in units of A.

Also refer to the following related links:
Op Amp Parameter Table
Op Amp Parameter Information

These pages were extracted from Op Amps For Everyone, Chapter 11, by Bruce Carter, Ron Mancini–Editor in Chief.
Copyright © 2000, Texas Instruments Incorporated