What is a Notch Filter?

Problem:
What is a Notch Filter?

Solution:
A Notch filter is a filter that passes all frequencies except those in a stop band centered on a center frequency. A closely related Knowledgebase item discusses the concept of the Q of a filter. This Knowledgebase item focuses on high Q notch filters - the type that eliminate a single frequency or narrow band of frequencies. A closely related type of filter - a band reject filter, is discussed in a separate knowledgebase item. The amplitude response of a notch filter is flat at all frequencies except for the stop band on either side of the the center frequency. The standard reference points for the roll-offs on each side of the stop band are the points where the amplitude has decreased by 3 dB, to 70.7% of its original amplitude.

The -3 dB points and -20 dB points are determined by the size of the stop band in relation to the center frequency, in other words the Q of the filter. The Q knowledgebase item will have additional information, but it is hard to talk about the roll-off points of a notch filter without defining the Q, which is the center frequency divided by the bandwidth. In the case of the figure below:




The phase response of a notch filter shows the greatest rate of change at the center frequency. The rate of change becomes more rapid as the Q of the filter increases.

The group delay of a notch filter is greatest at the center frequency, and becomes longer as the Q of the filter increases.

A common misconception of notch filter design: Many people think that the higher the Q, the deeper the notch. This is not true. The depth of the notch depends on the matching of components. The Q affects only the location of the -3 dB points, the stop band bandwidth. If the diagram above showed Q values of 0.01 and 0.001, the - 3 dB points would move outward, and the diagram would show a characteristic -20 dB per decade slope until the vicinity of the center frequency. Near the center frequency, the response would curve downward to the center frequency. A first order band rejection frequency would be created, but the response would only be first order with a sharp notch at the center frequency. This is not very useful, the designer would be far better off designing a band reject filter.