Sallen Key Notch Filter With Current Feedback Amplifiers

Problem:
How does a designer make an extremely high Q Sallen Key notch filter with current feedback amplifiers?

Solution:



The Sallen-Key circuit topology can be used to make an extremely high Q notch filter. This circuit is probably the highest Q notch filter that can be made with a single opamp. It has a lot of similarity with Twin-T filters:

Rf and R5 control both gain and Q. There is not controllability, however. Rf should never equal R5, or the circuit will become unstable. In practice, R5 should only be one or two standard values higher than Rf, which will constrain the range gain to just under 6 dB. Contact Texas Instruments applications for design techniques that will allow lower values of Q with this circuit topology.