Filter Design Wizard - Low Pass Filters

Problem:
How does a designer implement a low pass filter?

Solution:
When a low pass filter is implemented, there will be a range of frequencies from DC (or near DC) up, where the the amplitude is constant. Then, a slow roll-off will begin, which will increase to a final slope:



Design Procedure:
  1. Begin with the desired gain for the majority of the low frequency band (the flat region).
  2. Given that there will be roll-off at high frequencies, select the lowest frequency for which a 3 dB (or 70.8%) amplitude roll-off is acceptable.
  3. At ten times the frequency selected in the step above, is 20 dB (10 times rejection) acceptable, or would 40 dB (100 times rejection) be better?