Filter Design Wizard - High Pass Filters
Problem:
How does a designer implement a high pass filter?
Solution:
When a high pass filter is implemented, there will be a constant slope upward from low frequencies to high, which eventually becomes flat
to a constant amplitude:

Design Procedure:
- Begin with the desired gain for the majority of the high frequency band (the flat region).
- Given that there will be roll-off at low frequencies, select the lowest frequency for which a 3 dB (or 70.8%) amplitude roll-off is
acceptable.
- At one tenth the frequency selected in the step above, is 20 dB (10 times rejection) acceptable, or would
40 dB (100 times rejection) be better?