What is a Single Pole Filter?
Problem:
What is a Single Pole Filter?
Solution:
A Single Pole filter is a filter that rolls off frequencies in the stop band 20 dB per decade.
This is an example of a 10 kHz single pole low pass filter:

This is an example of a 10 kHz single pole high pass filter:

The pass band is the range of frequencies that are passed until the point is reached where the amplitude is rolled off 3 dB, or 70.7%. At ten times that frequency (for
a low pass filter), and one tenth the frequency (for a high pass filter), the amplitude is rolled off 10 times, or 20 dB. Thereafter, the amplitude is rolled off 20 dB
per decade of frequency.