spacer
OTHER KNOWLEDGEBASES
DSP TECHNICAL INFO
DSP RESOURCES
OMAP™ TECHNICAL INFO
OMAP™ RESOURCES
Analog Mix-Sig TECH INFO
Analog Mix-Sig RESOURCES
Logic TECHNICAL INFO
Logic RESOURCES
SC TECHNICAL INFO
SC RESOURCES
Digital Signal Processors
OMAP™ Processor Platform
Analog & Mixed-Signal
Digital Signal Processors
ADDITIONAL SC PRODUCTS
DESIGNED FOR TI DSP
HOW TO PURCHASE
CONTACTS
GENERAL QUESTIONS
  
  Have you visited the Tech Support KnowledgeBase?
Texas Instruments has gathered specific resources about our product groups into an easily searchable format. Specific areas for DSP, Analog, and Logic parts give you the fastest access to technical answers. more
 
  
MSP430: Multiplexing of MSP430 pins between JTAG and I/O functions

Problem:
How is it possible to share pins on some MSP430x1xx devices 
between JTAG and I/O functions?


Solution:
Four pins, P1.7 - P1.4 have both I/O and JTAG functions on 
the 20 and 28-pin MSP430F1xx devices. The default function for 
these pins is the I/O function when the device is powered up. 
When the Test pin is pulled high, these pins are selected as JTAG. 
The FET tools for those devices puts these pins in JTAG mode when 
using the interactive in-system debugger. Please see the FET tool 
User`s Guide for information on releasing the pins from JTAG mode 
while using the debugger.  

Note: If external circuitry is attached to the shared pins the 
interaction of the JTAG signals to the pins must be considered.  

If the device will be programmed or debugged interactively in-system 
via JTAG, consider what effect the circuitry will have. Take into 
account if the circuitry will load or bias the shared pins and 
thereby interfere with JTAG communications. Higher pin count devices 
have dedicated JTAG pins used only for debug and programming.



SURVEY

Did the information in this article help answer your question?

Yes
NO
NO, EMAIL TECHNICAL SUPPORT


Please provide additional comments about this information.
(255 character max)



(OPTIONAL) Please tell us how to get in touch with you:
Name
E-mail

Last Query: MSP430 (TM) Low Power Microcontroller

Session Log:
New Knowledge Server Session
Knowledge Base: dsp
Problem Selected
MSP430 (TM) Low Power Microcontroller
Solution (case) Considered
MSP430: Accuracy of the MSP430`s built-in temperature sensor
Solution (case) Considered
MSP430: Differences between MSP430x337 and MSP430x337A USART modules
Solution (case) Considered
MSP430: Stabilizing the DCO in the Basic Clock module of the MSP430
Problem Selected
Free Evaluation Tool problems
Solution (case) Considered
MSP430: Multiplexing of MSP430 pins between JTAG and I/O functions
Solution (case) Considered
MSP430: Sink and source current of MSP430 I/O pins
Solution (document) Considered
Configuration issues with C3x Code Composer Free Eval Tools from Web site
Solution (document) Considered
Getting error "Trouble Writing Target DSP memory" when loading code into C3x Code Composer Simulator ( Free Eval Tools).
Solution (document) Considered
Getting error "Trouble Writing Target DSP memory" when loading code into C3x Code Composer Simulator ( Free Eval Tools).
Solution (case) Considered
MSP430: Differences between MSP430x337 and MSP430x337A USART modules
Solution (case) Considered
MSP430: Sink and source current of MSP430 I/O pins
Problem Selected
Free Evaluation Tool problems
Problem Selected
MSP430 (TM) Low Power Microcontroller
Solution (case) Considered
MSP430: Stabilizing the DCO in the Basic Clock module of the MSP430
Solution (document) Considered
Configuration issues with C3x Code Composer Free Eval Tools from Web site
Solution (case) Considered
MSP430: Multiplexing of MSP430 pins between JTAG and I/O functions
'>