spacer
OTHER KNOWLEDGEBASES
DSP TECHNICAL INFO
DSP RESOURCES
OMAP™ TECHNICAL INFO
OMAP™ RESOURCES
Analog Mix-Sig TECH INFO
Analog Mix-Sig RESOURCES
Logic TECHNICAL INFO
Logic RESOURCES
SC TECHNICAL INFO
SC RESOURCES
Digital Signal Processors
OMAP™ Processor Platform
Analog & Mixed-Signal
Digital Signal Processors
ADDITIONAL SC PRODUCTS
DESIGNED FOR TI DSP
HOW TO PURCHASE
CONTACTS
GENERAL QUESTIONS
  
  Have you visited the Tech Support KnowledgeBase?
Texas Instruments has gathered specific resources about our product groups into an easily searchable format. Specific areas for DSP, Analog, and Logic parts give you the fastest access to technical answers. more
 
  
RTA failure in CCS 2.20

Problem:
Why does RTA fail in CCS 2.20 while RTA works fine for the same application in CCS 2.12?

Solution:
This FAQ applies to CCS 2.2 for C6000

RTA failure in CCS 2.20 is due to the change in the RTDX implementation between CCS 2.12 and CCS 2.20 that led to changes in target and host side emulation drivers. So the application needs to be rebuilt in CCS 2.20 to use the new RTDX libraries. This will make sure that RTA works.

If third party emulators are used, the respective drivers will need to be updated to incorporate the changes in RTDX implementations.


SURVEY

Did the information in this article help answer your question?

Yes
NO
NO, EMAIL TECHNICAL SUPPORT


Please provide additional comments about this information.
(255 character max)



(OPTIONAL) Please tell us how to get in touch with you:
Name
E-mail

Last Query: Code Composer Studio v2.2

Session Log:
New Knowledge Server Session
Knowledge Base: dsp
Problem Selected
Code Composer Studio v2.2
Solution (case) Considered
CCS installed on the desktop and laptop
Solution (document) Considered
Analysis Toolkit for Code Composer Studio v2.2 User's Guide (Rev. A)
Solution (case) Considered
DSP/BIOS Support in C2000 PC Code Composer Studio v2.2
Solution (case) Considered
CCS warning message "defined symbol can not have a .ref"
Solution (case) Considered
CCS doesn't work on Windows 2000 or Windows XP as standard user
Solution (case) Considered
RTA failure in CCS 2.20
Problem Selected
Code Composer Studio v2.2
Solution (case) Considered
CCS installed on the desktop and laptop
Solution (case) Considered
CCS doesn't work on Windows 2000 or Windows XP as standard user
Solution (document) Considered
Analysis Toolkit for Code Composer Studio v2.2 User's Guide (Rev. A)
Solution (case) Considered
DSP/BIOS Support in C2000 PC Code Composer Studio v2.2
Solution (case) Considered
RTA failure in CCS 2.20
'>