spacer
OTHER KNOWLEDGEBASES
DSP TECHNICAL INFO
DSP RESOURCES
OMAP™ TECHNICAL INFO
OMAP™ RESOURCES
Analog Mix-Sig TECH INFO
Analog Mix-Sig RESOURCES
Logic TECHNICAL INFO
Logic RESOURCES
SC TECHNICAL INFO
SC RESOURCES
Digital Signal Processors
OMAP™ Processor Platform
Analog & Mixed-Signal
Digital Signal Processors
ADDITIONAL SC PRODUCTS
DESIGNED FOR TI DSP
HOW TO PURCHASE
CONTACTS
GENERAL QUESTIONS
  
  Have you visited the Tech Support KnowledgeBase?
Texas Instruments has gathered specific resources about our product groups into an easily searchable format. Specific areas for DSP, Analog, and Logic parts give you the fastest access to technical answers. more
 
  
CCS warning message "defined symbol can not have a .ref"

Problem:
Why does CCS generate a warning message "defined symbol can not have a .ref"? This warning message was not generated in earlier versions.

Solution:
ISA: C6000; All CCS after v2.20:
This warning message is generated whenever a `.ref` directive is used to reference a symbol in an assembly file included using an `.include` directive; the symbol being defined using the `.equ` directive in the source assembly file.

This symbol should be used in the included assembly file without the `.ref` directive. The removal of the `.ref` directive in the included assembly file will eliminate this warning message. This non-requirement of the `.ref` directive in the included assembly file is detected only by CCS 2.20 and hence the other versions do not generate this warning message.


SURVEY

Did the information in this article help answer your question?

Yes
NO
NO, EMAIL TECHNICAL SUPPORT


Please provide additional comments about this information.
(255 character max)



(OPTIONAL) Please tell us how to get in touch with you:
Name
E-mail

Last Query: Code Composer Studio v2.2

Session Log:
New Knowledge Server Session
Knowledge Base: dsp
Problem Selected
Code Composer Studio v2.2
Solution (case) Considered
CCS warning message "defined symbol can not have a .ref"
Solution (case) Considered
CCS warning message "defined symbol can not have a .ref"
'>