spacer
OTHER KNOWLEDGEBASES
DSP TECHNICAL INFO
DSP RESOURCES
OMAP™ TECHNICAL INFO
OMAP™ RESOURCES
Analog Mix-Sig TECH INFO
Analog Mix-Sig RESOURCES
Logic TECHNICAL INFO
Logic RESOURCES
SC TECHNICAL INFO
SC RESOURCES
Digital Signal Processors
OMAP™ Processor Platform
Analog & Mixed-Signal
Digital Signal Processors
ADDITIONAL SC PRODUCTS
DESIGNED FOR TI DSP
HOW TO PURCHASE
CONTACTS
GENERAL QUESTIONS
  
  Have you visited the Tech Support KnowledgeBase?
Texas Instruments has gathered specific resources about our product groups into an easily searchable format. Specific areas for DSP, Analog, and Logic parts give you the fastest access to technical answers. more
 
  
What the error message "can't initialize target" indicates and how to fix it.

Problem:
This FAQ deals with the error message "can't (cannot) initialize target" and how to trouble shoot the problem.

Solution:
To Debug or Emulate any hardware board such as a DSK, EVM or custom board requires communication from the Code Composer (or Code Composer Studio) software to the DSP on the board. A failure or incorrect setting in any of the communication interfaces between the software and board will result in an error message from Code Composer as "can't initialize target". There are many possible reasons for the error as defined below:
---1. Communication between the Software (Code Composer) and Computer. For Code Composer to operate correctly, it must be loaded on an operating system the version supports. As a rule of thumb, TI will support popular operating systems that exist at the release of the Version. You can check what OSs are supported by viewing the Release notes located on the Code Composer CD-ROM
.---2. Communication between the Computer and the Emulator (XDS-510) or Development Board. Depending on what emulator or development board you are using (TI or Third Party), make sure that JTAG emulation can communicate with the Computer and Software you are using. Most Third Party Emulators or boards will include an Emulator Driver for Code Composer, and TI emulator or board Drivers are included with Code Composer. Load Code Composer with the proper Driver. Utilities are included with most emulators to perform a communication test.
---3. Communication between the Emulator and the Target board (non DSK or EVM). For the Emulator to communicate with the Target board, you will need a proper JTAG Header. The header should be attached according to the JTAG/MPSD Emulation Technical Reference.
---4. Communication between the Target board and the DSP (EVM or DSK). Many development boards will include Jumpers that configure the Communication Modes or Peripherals of the Board. Make sure that the Jumper settings are configured for Emulation when you connect them to the Computer or Emulator. The EVM or DSK tutorials included on the Tools Software CD-ROM will elaborate on these settings.
---5. Communication between the Software and the DSP. Finally, make sure that the Code Composer is running the right driver for the specific DSK, EVM, or Device. If communication has been successful using another board, DSP, or Version of software, look exclusively at the conditions that have changed.

For addtional information, please see the following User's Guide for further details: Emulation Fundamentals for TI DSP http://www-s.ti.com/sc/techlit/spra439.pdf


SURVEY

Did the information in this article help answer your question?

Yes
NO
NO, EMAIL TECHNICAL SUPPORT


Please provide additional comments about this information.
(255 character max)



(OPTIONAL) Please tell us how to get in touch with you:
Name
E-mail

Last Query: Initializing the Target DSP

Session Log:
New Knowledge Server Session
Knowledge Base: dsp
Problem Selected
Initializing the Target DSP
Solution (case) Considered
Locating or Identifying a Software Bug for TI Tools and Hardware
Solution (document) Considered
Getting the error "Data Verification Failed at 'address'" when loading an executable onto the target using File-Load Program
Solution (case) Considered
What the error message "can't initialize target" indicates and how to fix it.
Solution (case) Considered
C6211 DSK "Can't Initialize Target" error
Problem Selected
Initializing the Target DSP
Solution (document) Considered
Getting the error "Data Verification Failed at 'address'" when loading an executable onto the target using File-Load Program
Solution (document) Considered
Cannot initialize the TI emulator using emurst on a Solaris machine.
Solution (document) Considered
Error can't initialize target system (C5X)
Solution (case) Considered
Locating or Identifying a Software Bug for TI Tools and Hardware
Custom Page Viewed
Page: NavBar
Variable Updated
Variable: OBJECTNUMBER
Value: 2767
Custom Page Viewed
Page: NavBar
Variable Updated
Variable: OBJECTNUMBER
Value: 2767
Solution (document) Considered
Getting the error "Data Verification Failed at 'address'" when loading an executable onto the target using File-Load Program
Solution (case) Considered
Locating or Identifying a Software Bug for TI Tools and Hardware
Solution (case) Considered
C6211 DSK "Can't Initialize Target" error
Solution (document) Considered
Getting the error "Data Verification Failed at 'address'" when loading an executable onto the target using File-Load Program
Solution (document) Considered
Error can't initialize target system (C5X)
Solution (case) Considered
What the error message "can't initialize target" indicates and how to fix it.
'>