spacer
OTHER KNOWLEDGEBASES
DSP TECHNICAL INFO
DSP RESOURCES
OMAP™ TECHNICAL INFO
OMAP™ RESOURCES
Analog Mix-Sig TECH INFO
Analog Mix-Sig RESOURCES
Logic TECHNICAL INFO
Logic RESOURCES
SC TECHNICAL INFO
SC RESOURCES
Digital Signal Processors
OMAP™ Processor Platform
Analog & Mixed-Signal
Digital Signal Processors
ADDITIONAL SC PRODUCTS
DESIGNED FOR TI DSP
HOW TO PURCHASE
CONTACTS
GENERAL QUESTIONS
  
  Have you visited the Tech Support KnowledgeBase?
Texas Instruments has gathered specific resources about our product groups into an easily searchable format. Specific areas for DSP, Analog, and Logic parts give you the fastest access to technical answers. more
 
  
MSP430: Requirement of an external capacitor for ADC12 module of the MSP430

Problem:
Is an external capacitor needed on the VeREF+, VREF+ or 
VREF-/VeREF- pins of the ADC12 module?


Solution:
If you are using an external reference or one of the internal 
references for the positive reference, then  a 5-10uF capacitor
is required on pin VeREF+ or VREF+. If you are using an external 
reference for the negative reference, then a 5-10uF capacitor is 
required on pin VREF-/VeREF-. However, if you use AVCC as the 
positive reference, then no capacitor is required on pin VREF+ 
or VeREF+ and if you use AVSS as the negative reference, then no 
capacitor is required on pin VREF-/VeREF-. When using the AVcc 
and AVss as references the power supply decoupling capacitor 
provides the necessary low impedance path. Please refer the ADC12 
Grounding and Noise Considerations section under the ADC12 chapter 
in the MSP430xxxx User`s guide for more details.



SURVEY

Did the information in this article help answer your question?

Yes
NO
NO, EMAIL TECHNICAL SUPPORT


Please provide additional comments about this information.
(255 character max)



(OPTIONAL) Please tell us how to get in touch with you:
Name
E-mail

Last Query: MSP430 (TM) Low Power Microcontroller

Session Log:
New Knowledge Server Session
Knowledge Base: dsp
Problem Selected
Code Composer Studio v2.2
Problem Selected
MSP430 (TM) Low Power Microcontroller
Solution (case) Considered
MSP430: Stabilizing the DCO in the Basic Clock module of the MSP430
Solution (case) Considered
MSP430: Requirement of an external capacitor for ADC12 module of the MSP430
Solution (case) Considered
MSP430: Information sources for the MSP430 ADC12 module
Solution (case) Considered
MSP430: Differences between MSP430x337 and MSP430x337A USART modules
Solution (case) Considered
MSP430: Use of the port pins P1.4 - P1.7 on the MSP430x11x(x)
Solution (case) Considered
MSP430: Requirement of an external capacitor for ADC12 module of the MSP430
'>