spacer
OTHER KNOWLEDGEBASES
DSP TECHNICAL INFO
DSP RESOURCES
OMAP™ TECHNICAL INFO
OMAP™ RESOURCES
Analog Mix-Sig TECH INFO
Analog Mix-Sig RESOURCES
Logic TECHNICAL INFO
Logic RESOURCES
SC TECHNICAL INFO
SC RESOURCES
Digital Signal Processors
OMAP™ Processor Platform
Analog & Mixed-Signal
Digital Signal Processors
ADDITIONAL SC PRODUCTS
DESIGNED FOR TI DSP
HOW TO PURCHASE
CONTACTS
GENERAL QUESTIONS
  
  Have you visited the Tech Support KnowledgeBase?
Texas Instruments has gathered specific resources about our product groups into an easily searchable format. Specific areas for DSP, Analog, and Logic parts give you the fastest access to technical answers. more
 
  
C6211 DSK "Can't Initialize Target" error

Problem:
"Can't Initialiaze Target" error when trying to invoke the C6211 DSK.

Solution:
With regards to the C6211 DSK problems, please do the following:

* For Windows NT users, go into your CMOS setup when booting up your machine and configure the LPT for SPP mode. Make sure that the parallel port cable is not connected on boot up when doing the CMOS setup and make sure that the DSK is not powered on.
* Be sure to install the updated S/W that came in the floppy disk. (This is specific to v1.05 of the product).
* Setup the parallel port so that it is configured correctly and make sure the ports are set in the autoexec.bat.
* Configure the reset with the right value of the port address.
* The port setting should be either 0xa, 0xb, 0xc, or 0xd, depending on how the parallel port is set up and which port you are using.
* Go into CCS Setup and select the properties for the board listed under My System, make sure that the I/O port matches the setting that the reset works with (eg 0x0a).
* Under the Processor Configuration tab, remove the current CPU_1 (this would be the normal setting for the first CPU on a board) and add a single TMS320C6x1x to the system. This is driver is specific to the DSK. The TMS320C6x0x will not work with the DSK if it is selected.
* Save your settings and try again.

If CCS still doesn't come up, check to make sure that your path set to ;...C6000\DSK\BIN;...
and that you have the following files on your machine:

   XDSFAST1.SYS  in C:\winnt\ti
   XDSFAST2.DLL  in C:\ti\c6000\dsk\bin
   DSK6211.DLL   in C:\ti\c6000\dsk\bin
There should be an environment variable "unify_poddrvr_x=" with the above DSK6211 file name.
Always remember to reset the DSK before bringing up CCS.


SURVEY

Did the information in this article help answer your question?

Yes
NO
NO, EMAIL TECHNICAL SUPPORT


Please provide additional comments about this information.
(255 character max)



(OPTIONAL) Please tell us how to get in touch with you:
Name
E-mail

Last Query: Initializing the Target DSP

Session Log:
New Knowledge Server Session
Knowledge Base: dsp
Problem Selected
C6000 (TM) DSK FAQs
Problem Selected
Initializing the Target DSP
Solution (document) Considered
Why do the commands in my GEL functions seem to work intermittently?
Solution (document) Considered
Error can't initialize target system (C5X)
Solution (document) Considered
When launching Code Composer Studio, I am getting intermittent error messages indicating communication problems.
Solution (document) Considered
Emulation Fundamentals for TI's DSP Solutions
Solution (document) Considered
Getting the error "Data Verification Failed at 'address'" when loading an executable onto the target using File-Load Program
Solution (case) Considered
C6211 DSK "Can't Initialize Target" error
Solution (document) Considered
Cannot Initialize Target Error (C8X)
Solution (document) Considered
Getting the error "Data Verification Failed at 'address'" when loading an executable onto the target using File-Load Program
Solution (document) Considered
Emulation Fundamentals for TI's DSP Solutions
Solution (document) Considered
Cannot Initialize Target Error (C8X)
Solution (case) Considered
C6211 DSK "Can't Initialize Target" error
'>