spacer
OTHER KNOWLEDGEBASES
DSP TECHNICAL INFO
DSP RESOURCES
OMAP™ TECHNICAL INFO
OMAP™ RESOURCES
Analog Mix-Sig TECH INFO
Analog Mix-Sig RESOURCES
Logic TECHNICAL INFO
Logic RESOURCES
SC TECHNICAL INFO
SC RESOURCES
Digital Signal Processors
OMAP™ Processor Platform
Analog & Mixed-Signal
Digital Signal Processors
ADDITIONAL SC PRODUCTS
DESIGNED FOR TI DSP
HOW TO PURCHASE
CONTACTS
GENERAL QUESTIONS
  
  Have you visited the Tech Support KnowledgeBase?
Texas Instruments has gathered specific resources about our product groups into an easily searchable format. Specific areas for DSP, Analog, and Logic parts give you the fastest access to technical answers. more
 
  
CCS doesn't work on Windows 2000 or Windows XP as standard user

Problem:
CCS 2.2x doesn't work on Windows 2000 or Windows XP when the user is logged in with standard user privileges. Is there a way around this?

Solution:
CCS requires read and write access to specific registry keys when installing and using the product - specifically "HKCR" and "HKLM\Software\GODSP" and "HKLM\Software\Texas Instruments". Changes to the default security settings on Win2000 and WinXP mean that a standard "User" cannot run CCS.
Windows 2000 and Windows XP:
----------------------------
Code Composer Studio product needs to be installed using an account with Administrator privileges. If the installation process prompts for a reboot the administrator must log in again prior to first use. This will allow the installation process to update registry settings after a reboot.

However, the "Users" account under Windows 2000 is, by default, significantly more restricted than a "Users" account under Windows NT. One of the new restrictions is that the "Users" group has read-only access to all parts of the registry (except for HKEY_CURRENT_USER - which, at this time, we don't use).

During its normal course of operation, Code Composer Studio reads and writes configuration and session information to the registry. It also dynamically registers and unregisters COM components to ensure that the correct version of a CCS plugin is associated with a specific installation. There are two possible actions that may be taken to allow non-administrator users to use Code Composer Studio:

1. The administrator may modify registry permissions for the areas of
registry that are used by Code Composer Studio. The procedure to do this is
as follows:
	a) Log in as an administrator.
	b) Choose "Start->Run" from the Windows 2000 Start menu.
	c) Type "regedt32" (not "regedit") to bring up the Registry Editor.
	d) From the "Window" menu, select "HKEY_LOCAL_MACHINE on the Local Machine".
	e) Expand the "SOFTWARE" key.
	f) Locate and select the sub-key "GODSP".
	g) With "GODSP" selected, choose "Security Permissions." from the menu.
	h) In the upper half of the "Permissions for GODSP" window there will be a list of all the users and groups that access the key.
	i) Select the "Users" group.
	j) In the "Permissions:" box, locate the item "Full Control" and check the corresponding box under "Allow".
	k) Repeat steps "e" through "i" for "HKEY_LOCAL_MACHINE\Software\Texas Instruments" and "HKEY_CLASSES_ROOT"

2. The second option is to allow users that will be using the Code Composer
Studio product access via a "Power User" account. "Power User" accounts on
Windows 2000 provide an access level similar to that of a "User" account on
WinNT



SURVEY

Did the information in this article help answer your question?

Yes
NO
NO, EMAIL TECHNICAL SUPPORT


Please provide additional comments about this information.
(255 character max)



(OPTIONAL) Please tell us how to get in touch with you:
Name
E-mail

Last Query: Code Composer Studio v2.2

Session Log:
New Knowledge Server Session
Knowledge Base: dsp
Problem Selected
Code Composer Studio v2.2
Solution (case) Considered
CCS doesn't work on Windows 2000 or Windows XP as standard user
Solution (document) Considered
Software Bug Tool
Solution (case) Considered
CCS warning message "defined symbol can not have a .ref"
Problem Selected
Anatomy of a DSP Data Sheet
Problem Selected
Code Composer Studio v2.2
Solution (document) Considered
Design Considerations
Solution (document) Considered
Anatomy of a Data Sheet
Solution (document) Considered
Mechanical Data
Solution (case) Considered
Visual Linker support in C2000 PC Code Composer Studio v2.2 release.
Solution (document) Considered
Electrical Characteristics
Solution (document) Considered
Electrical Characteristics
Solution (document) Considered
Design Considerations
Solution (document) Considered
Software Bug Tool
Solution (document) Considered
Mechanical Data
Solution (case) Considered
CCS warning message "defined symbol can not have a .ref"
Solution (case) Considered
CCS doesn't work on Windows 2000 or Windows XP as standard user
'>