spacer
OTHER KNOWLEDGEBASES
DSP TECHNICAL INFO
DSP RESOURCES
OMAP™ TECHNICAL INFO
OMAP™ RESOURCES
Analog Mix-Sig TECH INFO
Analog Mix-Sig RESOURCES
Logic TECHNICAL INFO
Logic RESOURCES
SC TECHNICAL INFO
SC RESOURCES
Digital Signal Processors
OMAP™ Processor Platform
Analog & Mixed-Signal
Digital Signal Processors
ADDITIONAL SC PRODUCTS
DESIGNED FOR TI DSP
HOW TO PURCHASE
CONTACTS
GENERAL QUESTIONS
  
  Have you visited the Tech Support KnowledgeBase?
Texas Instruments has gathered specific resources about our product groups into an easily searchable format. Specific areas for DSP, Analog, and Logic parts give you the fastest access to technical answers. more
 
  
MSP430: In-system flash programming or usage as EEPROM.

Problem:
Can the MSP430 flash memory be programmed in-system, while 
executing code from Flash, or be used as EEPROM?


Solution:
The MSP430 is capable of programming in-system any single bit, 
byte or word anywhere in flash memory. Flash can be programmed 
in-system, even while executing code from Flash and even while the 
program is executing code from a segment being programmed. A segment 
does not have to be erased pior to programming, but 1`s can only be 
programmed to 0`s. Erasing is done on complete segments and erases 
all bit`s in the segment to 1`s. In-system Flash programming or 
erasing can occur while executing code from Flash, the program counter 
is automatically stopped during the operation for the duration 
specified in the device datasheet. As an option, the program counter 
can be moved to RAM and execute an application program during Flash 
in-system programming or erasing - in this case code continues to 
execute full speed, from RAM. Both the information memory and main 
memory flash areas can be used for either data or code or both. The 
only difference is that information memory consists of smaller 128 
byte segments whereas the main memory consists of 512 byte segements. 
A higher voltage is not required to program flash, though there is a 
restricted Vcc minimum specified in the device datasheet. Please see 
the flash chapter of the User`s Guide, application reports on the 
web and the device specific data sheet for more information on MSP430 
flash memory.



SURVEY

Did the information in this article help answer your question?

Yes
NO
NO, EMAIL TECHNICAL SUPPORT


Please provide additional comments about this information.
(255 character max)



(OPTIONAL) Please tell us how to get in touch with you:
Name
E-mail

Last Query: MSP430 (TM) Low Power Microcontroller

Session Log:
New Knowledge Server Session
Knowledge Base: dsp
Problem Selected
TI DSP Resources
Problem Selected
Code Composer Studio v2.2
Problem Selected
MSP430 (TM) Low Power Microcontroller
Problem Selected
Initializing the Target DSP
Solution (document) Considered
Cannot initialize the TI emulator using emurst on a Solaris machine.
Solution (document) Considered
Emulation Fundamentals for TI's DSP Solutions
Solution (document) Considered
Why do the commands in my GEL functions seem to work intermittently?
Solution (document) Considered
Error can't initialize target system (C5X)
Solution (document) Considered
After installing C6701 EVM, default GEL's to initialize the DSP gives errors and causes CCS to hang.
Custom Page Viewed
Page: NavBar
Variable Updated
Variable: OBJECTNUMBER
Value: 1891
Solution (document) Considered
Getting the error "Data Verification Failed at 'address'" when loading an executable onto the target using File-Load Program
Custom Page Viewed
Page: NavBar
Variable Updated
Variable: OBJECTNUMBER
Value: 4870
Custom Page Viewed
Page: NavBar
Variable Updated
Variable: OBJECTNUMBER
Value: 4954
Solution (case) Considered
MSP430: In-system flash programming or usage as EEPROM.
Solution (case) Considered
MSP430: IAR Embedded Workbench error message: unable to open file `cl430`
Solution (case) Considered
MSP430: Speed of the MSP430 SPI or UART
Solution (case) Considered
MSP430: Hardware USART configuration of the MSP430
Solution (case) Considered
MSP430: In-system flash programming or usage as EEPROM.
'>